GANTRY.PL.ERRWTHRESH

Description

If this value is not equal 0 and the position error GANTRY.PL.ERR is larger than this value, the drive will generate a warning.

If GANTRY.PL.ERRWTHRESH is set to 0 the warning is not issued.

Versions

Action Version Notes
Implemented 02-02-02-000  

General Information

Type Read/Write
Description Sets the position error warning level for Gantry Mode.
Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range Depends on units. See Position Range for details.
Default Value 0 counts
Data Type Float
See Also AXIS#.PL.FB
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.